Part Number: CC1101 Team,
1) Looking at the CC1101EMK868-915 kit ( https://www.mouser.fr/new/texas-instruments/ti-cc1101emk868-915-development-kit/ ):
Q:What module is provided in this kit? Is it: http://www.ti.com/tool/CC1101CC1190EMK915 or http://www.ti…
Other Parts Discussed in Thread: CC1101 Hi,
I have a set of CC1101DK433 development kit and want to interface external peripheral devices to 8051. I want to configure 8051 to get data from the peripheral devices and send to CC1101 for RF transmission…
Hi,
Can anyone clearly explain how to make bootloader compliant code for running custom software in CC1101DK433 in Keil C51. Although, the document has separate section on this, it is not clear.
Thanks,
Vignesh
Hi,
I have the CC1101DK433 with two EB and two EM.
I found some examples (C51 for smartrf04) from the TI web site but I'm not able to try them.
I read the " example and libraries" pdf but in my SmartRF04 Studio I can't find the button Load USB firmware…
It is possible to change the link examples of the CC1101DK433 kit development to show the RSSI values? does this require an additional programmer to program the silabs MCU? Thanks.
Other Parts Discussed in Thread: CC1101 Hi,
I am trying to use the synchronous serial mode on the CC1101DK433 development board. I am transmitting from one board and I have used an oscilloscope to check the GDO0 pin on the receive board. Sure enough, I…
Thanks!
I was looking at CC1101DK quick satrt guide - SWRU126B but I am not 100% sure: -Do you mean that CC1101DK433 and CC1101DK868-915 are the same HW kit? -Is just a SW change needed to operate the kit in 868-915MHz band? -Are both antenna types (868…
Hi,
1. Make sure the module you are using has a RF filter for 433MHz. You can use SmartRF studio with another sub-1G device to see if your frequency is at 433MHz. Use the Continuous RX tab with base frequency set to 433MHz and look at the RSSI. This…
CC1101DK433 consists of two boards; CC1101EM-433 and SmartRF04EB.
EM: A small module containing CC1101 and the needed external components (crystal, supply decoupling, balun, filtering)
EB: A motherboard which contains various user interface circuitry…
About RF performance test of CC1101DK433, the RX dynamic range is from 0dBm to -95dbm (BER cretiria is 5 % ) , @ 403MHz , GFSK , 76 KBaud ;
But the bug is, when the RSSI = -76dBm , BER behaves worse , up to 12%.