Hi
Am trying to put the temperature data in a packet and to tx/rx that packet....
but am getting the above attached error...
could anyone suggest some solution for this...
If anyone could help me i would appreciate it very much.
The time it does to load samplelight example is 2.30 min
With uniflash which i tried i had the same problem.So is there a possibility to be normal?
Other Parts Discussed in Thread: CC2538 Hi
I am working on cc2538 PER test firmware....I have some doubts...could anyone please clarify.....
unsigned char txPower; unsigned long burstSize; unsigned long pktRate; unsigned char gainMode;
Could anyone…
Other Parts Discussed in Thread: CC2538 , CC2538-SW Hi
can anyone give a snippet code for cc2538 board for interrupt without polling....?
I have seen a sample code for gpio but that code uses polling method which is not usable for my project.....
Other Parts Discussed in Thread: CC2538 Dear TI,
I need the cc2538 Evaluation Modules dimentions, PCB width and height in mm
and the cc3000Boost PCB too. It isn´t in the users guide
Thank you in advance
Hi Jim,
I had a similar problem when trying the devices in our Lab, after having ensure the code by trying it at home, the only possibility is that either the network used in the university does not allow connections that are not verified (i.e. MAC…
I am trying to put the system in PM2 and wake it up by pin interrupt. For this purpose I am using the power-up interrupt in contiki and it is working but it wakes up and goes to the ISR of the corresponding port and stays there. I am thinking that the…
Other Parts Discussed in Thread: SYSCONFIG Hi Team,
Can you please check and advise with request?
"
I am working on the RF Serial boot loader but it is not working. I followed the configuration that are in the attached document, but it is still…
Other Parts Discussed in Thread: CC2538 I have a custom board that is based on CC2538EM's schematics. When I connect the custom board to the SmartRF06eb's 10 pin JTAG connector, it outputs "Error 230".
Chapter 6 of SWRU345A describes 6 possible cases…