Part Number: CC3120 Other Parts Discussed in Thread: CC31XXEMUBOOST , UNIFLASH , Hi
I have a custom board with a CC3120 device in pre-regulated mode, which I am trying to bring up. All the power rails are OK.
I connected the CC3120 to a CC31xxEMUBOOST…
Hello Kristen,
Thanks for providing this link.
I've referred to the "Uniflash" section and found problem in my set-up.
When the CC31XXEMUBOOST is connected to the PC, it detects as QUAD COM ports and we need specifically select the third port to…
Wow, I feel like such a buffoon. I was very careful to line up the silk compared to the MSP430 Launchpad and then just assumed it went on the same way compared to the EMUBOOST. Turns out it flips orientation!
That fixed it. I was able to update the…
Other Parts Discussed in Thread: CC3100SDK , CC3100BOOST , CC31XXEMUBOOST How do I get the CC31XXEMUBOOST + CC3100BOOST to work in WPS mode. I see the example C:\ti\CC3100SDK\cc3100-sdk\examples\provisioning_wps\main.c. What do I need to do to get this…
Other Parts Discussed in Thread: CC3100BOOST , CC3100SDK , CC3100 Hi,
I've just received a CC31EMUBOOST and a CC3100BOOST board, and want to get started with them.
Following the "CC3100 SimpleLink™ Wi-Fi® and IoT Solution Getting Started Guide"…
Hi Javier, Sorry no. CC3100 need to be controlled by external device. It can be PC (via USB -> UART converter) or microcontroller via SPI or UART interface. Jan
Other Parts Discussed in Thread: CC3100 I'm trying to finish the SimpleLink Wi-Fi CC3100 Project 0: Microsoft Visual Studio example but after I connect to the AccessPoint the device fails to connect to the LAN. Here is the output:
Device is configured…
Other Parts Discussed in Thread: CC3100 , UNIFLASH , CC31XXEMUBOOST Hi,
We have a board of our own design that uses a cc3100. We need to flash the cc3100 using uniflash, and are getting errors. We have our cc3100 uart connected to the uart lines of…