Part Number: CDCI6214EVM I have a register configuration which i want to program into the EEPROM so that it would be automatically bought up to the device on power-up. I am using the TICS pro software to first program the register config to EEPROM.
…
Part Number: CDCI6214EVM Other Parts Discussed in Thread: USB2ANY Hi,
I'm trying to load my TICS Pro file onto my CDCI6214EVM board, the "USB2ANY" is connected and green, but when toggling the "PWR on/off" button, I get the "No Device Found!" pop-up.…
Part Number: CDCI6214EVM Other Parts Discussed in Thread: CDCI6214 Hi Team,
I wanted to know if it is possible to share with me the internal quarts resonant frequency within the CDCI6214EVM,
What is the quart's accuracy?
Also, when generating frequencies…
Part Number: CDCI6214EVM Hi,
Input is 25Mhz, require output frequency1 is 100Mhz,require output frequency2 is 100Mhz,require output frequency3 is 100Mhz,require output frequency3 is 19.2Mhz.
TICS Pro GUI set as below,is it right? Need The Block Diagram to be…
Part Number: CDCI6214EVM I am having the same issue as described here: https://e2e.ti.com/support/clock-timing-group/clock-and-timing/f/clock-timing-forum/680535/cdci6214evm-ticspro-issues
That issue is marked as resolved, but the resolution does not appear…
Part Number: CDCI6214EVM Other Parts Discussed in Thread: CDCI6214 , CDCE6214 Just loaded TICSPRO_SW want to use CDCI6214 device. How do I load device files?
Thanks
Part Number: CDCI6214EVM Where can I find any information on how to use the Wizard to set target frequencies? There are are two many options in the Wizard
Part Number: CDCI6214EVM Other Parts Discussed in Thread: CDCI6214 , CDCE6214 Hi Experts,
Good day. Allow me to paste the full query of my client:
I purchase a demo board of CDCI6214, I configured the CDCI6214 on demon board with software TICS Pro. When…
Part Number: CDCI6214EVM Other Parts Discussed in Thread: CDCI6214 Hello!
We're currently developing w/ the CDCI6214 for our solution. As we'll need to generate a requested frequency "on the fly", we can't use TICS to reprogram, so we need the I2C communications…
Part Number: CDCI6214EVM
Hello, I am proceeding to some tests in order to define wether we can work with your product in our project.
I try to store and recall settings into the EEPROM. After some testing I could understand more or less how it works. However…