Hello! The DLPC120-Q1 is part of a full chipset. On its own, it is only a controller, designed to format incoming video data to be properly displayed on the DMD. When paired with the DLP3030-Q1 and an LED driver, it can form the electronics portion of…
Hi Yu Dong,
Glad to hear that the change for R9 to one of the boards is working.
For the other board that is not working it looks like the configuration file is different between the one programmed into the piccolo MCU and the ASIC application flash…
Hi Johns,
Please see the attached user guide and go to section 5 on reprogramming the EVM. This outlines the recommended method and order of programming a completely blank TMS320f28023. You should not need to use CCS and all steps can be performed with…
Hi,
For the first issue, to program the piccolo bootloader correctly using the DLPC120 control program I believe you need to have the uniflash.bat file be from the code composer studio directory. There are other files in the CCS directory that may be…
Hi Mr. Wang,
You should not be seeing a red light, are you able to connect to the DLPC120 control program and do you see any error messages or what does the System Information section say?
In terms of how to flash the system please see the following…
Hi,
I have attached a DLPC120 ACP user guide for reference as well as a guide on calibration.
7026.DLPU059_ACP_UsersGuide_March2018 (2).pdf
5226.DLPU066_Calibration_User_Guide_March2018 (3).pdf
The HUD Piccolo SW release contains Piccolo main…
Hi Weite,
1. I understand the CA210 may be hard to acquire or unavailable now and we recommend and can support the CA410 display color analyzer with the DLPC120 Control Program. We have not looked into or support the other tools you had mentioned. We…