Gyanendra,
Unfortunately, I do not believe it is possible to swap the DLP4500 DMD to have NIR coating. Really, such a thing already exists in the form of the DLP4500NIR DMD, which features a similar form factor but is rated for NIR (with the correct…
Hello Takeshi. How to upgrade from version 1.0 to version 2.0? Do we need to download DLP NIRscan MicroSD Image for Windows 2.0 from www.ti.com/.../dlpnirscanevm only?
Hello new user,
Welcome to the DLP Advanced Light Control section of the TI-E2E community.
Here is guidance recevied from the NIRscan team:
AM335x Sitara Bundle: open source SDK for the Sitara processor
DLP NIRscan Software Bundle for Linux –…
Adrien,
Welcome to the E2E forums, and thanks for your interest in our DLP technology.
In terms of software, you should check out the DLP4500NIR Nirscan software bundle (at www.ti.com/.../DLPNIRSCANEVM) , which may provide the pattern control you…
Tina,
The NIRscan EVM is a 4500NIR-based EVM, which comes with an associated reference design. The resources you are looking for can be found below:
www.ti.com/.../tida-00155
www.ti.com/.../dlpnirscanevm
I hope this helps.
Best Regards, …
Other Parts Discussed in Thread: DLPNIRSCANEVM , TIDA-00155 Hi!
I'm planing to order DLPNIRScanEVM but the users guide (page 10) shows that the system is designed to be used in transmission mode.
Is there available a spare part to replace the sample…
Allen,
I'm not sure that I'm understanding. Is there some documentation that you're reading that indicates that the DLP4500NIR is controlled by the Lightcrafter 4500? Or can be used in the Lightcrafter 4500?
The evaluation model that we have for…
Paolo,
Welcome to the E2E forums, and thanks for your interest in our DLP technology.
The DLP4500NIR DMD needs to be accompanied by the DLPC350 controller as part of a full DLP system. To faciliate design of a system using these components, we have…
Hello User,
Welcome to the E2E forum and thank you for your interest in DLP® technology.
The DLP4500NIR has an EVM, the DLPNIRSCANEVM . However, I would not say that this is a low cost setup. Support software can be found on the DLPR350 page .
dotan…
Hello,
It is possible to connect an Raspberry Pi to the NIRscan Nano EVM. You may wish to refer to this thread where a client inquires after a similar implementation:
https://e2e.ti.com/support/dlp-products-group/dlp/f/dlp-products-forum/804154/dlpnirscanevm…