Part Number: DRV10983Q1EVM Other Parts Discussed in Thread: USB2ANY
Hi Ti Expert,
We are using motor controller DRV10983Q1EVM and connected it with USB2ANY. The application is DRV10983Q1 EVM GUI.
We are operating a 3 phase BLDC motor. After giving…
Part Number: DRV10983Q1EVM Other Parts Discussed in Thread: USB2ANY , DRV10983 Hi TI expert,
We are using DRV10983Q1EVM with USB2ANY ( part no. HPA665-001) . The GUI is DRV109XXEVM.
When we open the application we get an error message saying "Register…
Part Number: DRV10983Q1EVM
Hi team,
According to the specification, the motor speed can be controlled by PWM in three ways. However, after the motor is controlled by GUI software, I made the following Settings, none of which can control the motor speed…
Part Number: DRV10983Q1EVM Other Parts Discussed in Thread: DRV10983-Q1 Hello, I am testing the drive with 1 pole pair high speed motor for possible remote controlled device. During the tune up procedure I was using DRV10983Q1 EVM GUI ver. 3.3.4 (latest…
Part Number: DRV10983Q1EVM Hi team,
I think there is GUI (DRV109xxEVM) that able to control and change parameter of the board,
but after start this GUI, there is the error message which tell us it cannot find Labview run time engine.
I already downloaded…
Part Number: DRV10983Q1EVM Other Parts Discussed in Thread: DRV10983EVM We used a DRV10983Q1EVM evaluation board, the tuning guide and the TI GUI to find parameters that will work for our motor and requirements. The motor ran as expected, but as soon…
Part Number: DRV10983Q1EVM We are looking for eval board to test our motor
small highspeed motor
sensor less, brushless
1 pole pare
24v
1.5 amp
150,000 rpm
adjustable speed needed.
Part Number: DRV10983Q1EVM Other Parts Discussed in Thread: DRV10983-Q1 , DRV10975 , Please consult the team DRV10983Q1. During the motor operation, the motor was loaded into 1A current DRV10983Q1 and the protective stop was performed. What is the problem…
Part Number: DRV10983Q1EVM Other Parts Discussed in Thread: DRV10983-Q1 , DRV8320 , DRV10983 Hello guys,
I have a motor whose parameters are described in the attached picture. The motor phase to phase resistance is 60.2OHM which after dividing with 2 will…
Part Number: DRV10983Q1EVM Other Parts Discussed in Thread: DRV10983 , DRV10983-Q1 , USB2ANY I have EMAX2216-810KV brushless motor which I am trying to run using DRV10983_Q1EVM module but unfortunately, I don't have any parameters or data related to the…