Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: DRV8301 I would like to get maximum torque on low speed & high speed sensored motor control, on LAB 13b I'm able to do the position control and speed control very well, but seem that current…
Part Number: LVSERVOMTR Other Parts Discussed in Thread: DRV8301-69M-KIT Hello,
we are evaluating the dynamometer and wonder if LVSERVOMTR digital encoder can be plug straight to eQEP interface on DRV8301-69M-KIT board.
I can not find the wiring and…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: DRV8301 Hello,
I want to control the driver thanks to Arduino and not Piccollo controler in my application.
I'm just starting and I want to see what's happened when I set a value on PWM_AH…
Part Number: DRV8301-69M-KIT Regarding the function
STVELPLAN_setCfgState (ST_VELPLAN_Handle handle, uint16_t StateIdx, _iq24 VelEnd, int32_t Timer_tick)
For my application, I cannot stay in a state for a fixed time. If the conditions are satisfied…
Part Number: DRV8301-69M-KIT In this function STVELCTL_setAxis(obj->velCtlHandle, ST_AXIS0); what this AXIS?, whether it is q-axis/d-axis or some other thing.
Thanks
Vivishekh
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: TMS320F2806 , DRV8301 , MOTORWARE , TMS320F28069 Hello,
I am testing on evaluation board DRV8301-69m-kit, with
As soon i power up with 24 Vdc power supply the Fault LED corresponding to…
Part Number: DRV8301-69M-KIT Dear team:
When the customer is testing the lab02b routine, the motor runs smoothly and can observe the saddle wave . Observe the output waveforms of each test point as follows.
One of 3 sets of PWMxH/L:
Test the 3…
Part Number: DRV8301-69M-KIT
How much variation / tolerance (in percentage) can be acceptable in the inductance value(Ls/Ld) for BLDC motor.
Thanks,
Vivishekh
Part Number: DRV8301-69M-KIT I am writing to inquire about the availability of any low cost instrumental cluster, Which can be support DRV8301-69M kit and Piccolo 28069 controller.
Regards,
Vivishekh sivan