FYI, we are looking at DRV8962DDVR as replacement in our application. It is actually much closer to the functionality of the DRV8432 than the suggested DRV8462.
Hey Kevin,
The best device for DC60V and 5A is the DRV8962 , which is in Preview right now but will be released (active) soon.
We don't have many integrated DC drivers for 60V, so I also recommend looking into using a gate driver instead such as the…
Hi Andrew,
Are there any updates? It's been almost a month and we have not heard back from you. I will close this thread for now but you can reply back if you need further assistance
Hey Maik,
Does this look right?
EVM User's Guide: DRV8432EVM Motor Drive Evaluation Board
DRV8432EVM User Guide.pdf
If you're driving a brushless (BLDC) motor I highly recommend checking out our BLDC product line instead. The DRV8432 device is…
Part Number: DRV8432EVM Other Parts Discussed in Thread: DRV8874EVM , DRV8412 , DRV8876 , DRV8874 I'm rather new to this field and want to apologize in advance for possibly stupid questions. I want to use the motor driver on a capacitive load at low frequencies…
Part Number: DRV8432EVM Hi team,
Could you please tell me why there 're some components which are not assembled on the EVM ? Such as C25 /C26 .
And What does these components do?
Regards,
Jhon Chen
Part Number: DRV8432EVM Hi,
When I used DRV8432EVM, I chose mode 3 to test the brushed DC motor, but when I disconnected the circuit, the oscilloscope showed that there was a large reverse voltage at both ends of the motor.
I wanted to know why and how…
Part Number: DRV8432EVM Hi Team,
I want to use DRV8432EVM to test brushed DC motor.
I really wonder if there is any relevant example or application.
Sincerely,
Jhon Chen
Part Number: DRV8432EVM Good day to you.
We received 2 type of box for this part. one is Red box (-> D/C 1539) and the other one is Blue Box (-> D/C 1712).
We would like to check this part is same spec or there are some differences for this.
Below…