Other Parts Discussed in Thread: CC430F6137 , RF430F5978 , CC430F5137 , RF430F5978EVM Hi ,I will buy your devkit for my project.
But i have some questions.Before my decision i have to know something about em430f5137rf900 or EM430F6137RF900 devkits.
my first…
I am wondering if it is possible to install Contiki on development board EM430F5137RF900? It is not among the supported TI hardware list on the contiki webpage but could it still support Contiki? Any information will be helpful. Thanks!
I also faced same issue with SmartRF Studio7 v1.14.2.1. And observed the issue resolved with the latest version(v1.15.0).
Please try to use the latest version( http://www.ti.com/tool/smartrftm-studio )
Best Regards, Enok
Other Parts Discussed in Thread: CC430F5137 Hi, I want to use EM430F5137RF900 as a SPI slave to connect with an OMAP board as master.
Because I am not familiar with SPI, I start from the MSP430 SPI example code. I use two EM430F5137RF900, one as the master…
Other Parts Discussed in Thread: SIMPLICITI Used the example project of SimpliciTI(CC430EM\Simple_Peer_to_Peer) with EM430F5137RF900 eval board, the LinkTo device can not sync. with LinkListen device?
The Red-LED on LinkListen device was ON and Green-LED was OFF…
Other Parts Discussed in Thread: CC430F5137 Hi,All,
Recently I got a pair of EM430F5137RF900 boards, I found out that there are two 32 KHz crystals in the kit. Though the footprint of the EM board has place for the 32 KHz crystal, they are not soldered…
I want to use the EM430F5137RF900 as a SPI slave.
Now I try to load one of the CC430F513x Code Examples (http://www.ti.com/litv/zip/slac458a) into CC430F513x using IAR for MSP430. The one I used is "cc430x513x_uscia0_spi_10.c". However, it seems…
We bought CC-6LOWPAN-DK-868 kit, and two EM430F5137RF900 are used as the node in the kit.
Since EM430F5137RF900 has 2 USCI ports, we want to connect the EM430F5137RF900 with other board via SPI.
According to the schematics of EM430F5137RF900 , it seems…
Hi MSP430s at TI.
I posted this request on the low power RF forum but they pointed me to here.
I was wondering if you are able to supply the actual Altium design files for the EM430F5137RF900? I don't want the gerber files. A customer of mine is…
Hi TI,
Is there any chance of getting my hands on the actual design files of the EM430F5137RF900 board? I don't want the gerbers, which can be downloaded form the public TI web-site, but instead the actual Altium pcb design files.
Thanks,
Mi…