Part Number: EVM430-FR6047 Hello Team,
Refer below table, it shows difference between inline & Clamp on type sensor. Kindly suggest can we interface clamp on type sensor to EVM430-FR6047?
Items
Inline Sensor
Fuji Electric FSSC
Installation…
Part Number: EVM430-FR6047 Hi,
i exported the 3 files from the GUI and I'm afraid that there is a definition in USS_Config.h that I don't define correctly because I always get the same value as:
can you help me?
I didn't change anything, this…
Part Number: EVM430-FR6047 Hi I currently use 1MHz sensors. The more I try to read the ADC on thick pipes, the more difficult it is I wanted to know if I should look for sensors of less than 1MHz? or more than 1MHz?
That is, the more I transmit at a higher…
Part Number: EVM430-FR6047 Hi!
I get this signal. I have a deviation towards the positive side. I can't find a parameter in the GUI that allows to adjust the deviation, I asked you before and you told me to look for a parameter: USS_APP_DC_OFFSET_CANCE…
Part Number: EVM430-FR6047 Other Parts Discussed in Thread: MSP430FR6047 hi
after switching variants to, i still get warning however, download does occur.
what can i do to remove this error.
Part Number: EVM430-FR6047 I have purchased EVM-430FR6047 for water metering application but while using it ,the lcd was not showing the quantity volume rather it was every time showing zero.How i can measure volume and please also show in source code…
Part Number: EVM430-FR6047 I am using EVM430-FR6047 for water meter application but while using it ,it doesnt show the volume measured on lcd.please tell why it is so, also please help if i want to make customised board for water meter using only mcu…
Part Number: EVM430-FR6047 Hello,
I am currently using a EVM430-FR6047 board to take TOF Level Sensing readings with a single transducer (SMD20TF1000R) which is glued onto a Graduated cylinder as depicted below. The goal is to have the program print out…
Part Number: EVM430-FR6047 I'm using MSP430-FR6047 PCB with USS Design Center and MSP430FR6047EVM_USS_Demo project.
Design Center GUI and demo project versions are 02_40_00_00.
I have some questions in USS Demo project.
(USS_Config\USS_userConfig…
Part Number: TIDA-01486 Other Parts Discussed in Thread: EVM430-FR6047 , , TS5A3357 Hello everyone, recently I wanted to use EVM430-fr6047 to design an ultrasonic flowmeter for use on stainless steel pipes, but the signal is weak, I noticed this design…