Other Parts Discussed in Thread: HDC1010EVM Hello
I do have a part number but for some reason, the PN HDC1010EVM i s not recognised in the "Part Number" field of this form,. This is strange because it is a valid part number and below is the manual for this…
Part Number: EM430F6137RF900 Good morning,
months ago I bought an HDC1000EVM evaluation kit.
I wolud like to download the software, but I can't find it.
Coluld you help me please?
Best regards
Paolo Lucardesi
MMT
lucardesi@mmtitalia.com
Part Number: HDC1000EVM SensingSolutionsGUI-1.9.2 dont detect HDC1000EVM on a W7 PC but it does on a W10 PC.
ìs it incompatible with W7 or is there a way to configure the GUI?
Part Number: HDC1000EVM Tool/software: Code Composer Studio HI,
I'm trying to build following project which exist under "../Sensing Solutions EVM GUI-1.8.8/EVM Firmware" folder.
* Project name : HDC1000_F5528_V0
However, I faced following…
I want to measure the humidity (amount of water vapor) that mixed in helium or nitrogen. Does this this sensor works perfectly in the medium other than air? Do you have any suggestions to calibrate this sensor for other medium (environment)?
Hi Steve,
Sorry this has gone without a response for so long. There is a newer version of the EVM GUI that should support Win8:
www.ti.com/.../snoc028
Sensing Solutions EVM GUI Tool v1.8.8 (Rev. A)
(ZIP, 60718 KB) 12 Oct 2015
Please let us know…
Hi Everyone,
We are working on a sensor based project & using HDC1000EVM for testing.
we got a lot of support from TI & e2e Forum. But, when we use the EVM & HDC1000EVM GUI , there is error in measurement upto 5 Degree
for reference we are…
Hi Everyone,
We are working on a sensor based project & using HDC1000EVM for testing.
we got a lot of support from TI & e2e Forum. But, when we use the EVM & HDC1000EVM GUI , there is error in measurement upto 5% RH
for reference we are using…
Other Parts Discussed in Thread: HDC1000 The USB driver for the HDC1000EVM is not installing during installation, where can I download the driver so I can install it manually? See attached screen shot. Note: I tried the install many times, all with the…