Other Parts Discussed in Thread: TM4C1294NCPDT Dear Sir.,
We need the High performance Tiva microcontroller as per the following specifications.
We are going to developing the Industrial Textile Machinery with High speed and High performance,
Already we…
Other Parts Discussed in Thread: CSD16570Q5B I am looking for a MOSFET capable of handling a current range from 0 to 600A, where the input voltages range from 0.4 to 1.4 volts. Can you suggest a MOSFET with very low on resistance (Rds) or a parallel configuration…
Hi Stefan,
there seems to be a difference between the previous circuit and our actual one: in our actual circuit the BOOT pins are connected to the VCC pin and separated from the 12V line which is only connected to BIAS and VIN. So this is not the origin…
Part Number: INA826 Other Parts Discussed in Thread: TPS2661 , In this app note: https://www.ti.com/lit/an/sbaa551/sbaa551.pdf what is the purpose of R1 and R9 on page 3. Also what type of capacitor would be best for this application (such as C4)? I was…
Part Number: LM5152-Q1 hi Friend,
When the IC output is low voltage, is it achieved by frequency reduction or other ways? In addition, if the output is high voltage, the IC is adjusted by what working principle?
Part Number: LAUNCHXL-CC1352P Other Parts Discussed in Thread: SYSCONFIG Hi,
I am using 2 LP-CC1352P1 to do some tests and later develop a project. I was testing RF performance in Sub-1 GHz network. The test consists on running the TI 15.4-Stack senso…
Part Number: LM48580 Other Parts Discussed in Thread: TLV320DAC3100 Hello TI Team,
I am seeking a cost-effective audio DAC compatible with the LM48580 for driving a piezo speaker. ( piezo specs: 24Vpp,1.0uF±30%,1kHz, 200mApp). Due to design constraints…
Hi,
The data is continuously set on the GPIO on the falling edge of the clock no matter how weak the RSSI is. So you need to constantly read and process the data on the rising edge of the clock. If you don't want to process the data all the time as…