Part Number: ADS5282EVM Other Parts Discussed in Thread: HSADC-SPI-UTILITY Hi,
when trying to install the HSADC-SPI-UTILITY software I get the following error
The PC is running Windows 10 64-bit. Software was downloaded recently (slac177d)
Any suggestions…
Hi Dave,
We recommend to keep the ADC and DAC powers separated.
For the DAC, if the customer truly wants to utilize the phase noise performance of this device, then they should replicate the DAC EVM power supply circuits 5X times.
For the ADC, you can…
Hello Chong,
You are correct that the maximum SPI clock frequency that is supported with the datasheet specifications is 18MHz. However, there is no association between the SPI frequency or data rate, and the CAN bit rate. The SPI data rate is based on…
Part Number: LM98640CVAL Hi,
We are requesting support files to utilize with the SPI host adapter that was supplied with the LM98640CVAL Evaluation Board. Supplied with the Eval board was a Total Phase Aardvark I2C/SPI Host Adapter. The LM98640CVAL Evaluation…
Part Number: AM62A7 I am new to the TI-processor SDK and kernel/driver level programming. My educational task is to run an app on AM62A7 to read an external ADC (ADS7049) via SPI interface.
I have the following information:
# Read value from ADC via SPI…
Part Number: TRF7964A Hi TI Team,
Project Overview
First time, I am Designing RFID/NFC Device.
This project for Warehouse management project.
RFID/NFC Distance : MAX 30 cm or Min 5 cm
Is this Right ic for this project ? if not please reference any ot…
Part Number: AM625 Hello,
I want to utilize an LTE 4G or 5G support chip on my AM625 SOM device. Please provide me with the steps to locate the driver support in the menuconfig, and identify the TI-supported chipset, either supporting SPI or SDIO.
Thanks…
Hi John,
Check into using the SN65LVDS31/33 - Figure 2. TIDA-060017 Block Diagram in the application note utilizes this solution.
Transmitting SPI Over LVDS Interface Reference Design
You can view other relevant files for this reference design here: TIDA…
For the ADS1178, MOSI and CS lines are unavailable. How can we establish an interface without these lines? Additionally, can alternative lines be utilized to connect to the MCU since we require four SPI lines? Can you please provide the answer.
Part Number: ADS1178 For the ADS1178, MOSI and CS lines are unavailable. How can we establish an interface without these lines? Additionally, can alternative lines be utilized to connect to the MCU since we require four SPI lines? Can you please provide…