It implements the XDS 110 functionality . CCS (or other supported IDE such as IAR) will update the firmware without your involvement.
You can also use external debugger probe such as https://www.ti.com/tool/TMDSEMU110-U .
Hi Kevin,
Are you building on IAR or CCS?
Please refer to the SDK quick start guide to check if you have performed the steps mentioned in there. Especially IAR needs update of argument variable.
https://dev.ti.com/tirex/content/simplelink_cc13xx_cc26xx_sdk_7_10_02_23…
OK quick update I did manually add an "iar" directory and put the startup file in there and the build worked. I think this is some sort of project setup issue with the template...
Munan
Part Number: CC2538 Other Parts Discussed in Thread: UNIFLASH , Z-STACK , CC2530 Tool/software: TI C/C++ Compiler Hi TI team
I had a very strange question:I use my previous develop zstack, it can use a IAR IDE update CC2538 firmware.
But why I can not use…
Hi ari,
Thank you for the update. I have been able to replicate your issue and recommend that you try using IAR v9.50.2 instead as I was able to correctly start a program and debug session using this version. Be sure to delete your prior workspace and…
Thank You Johnson,
It did help, partially.
I updated mspm0_sdk to mspm0_sdk_1_10_01_05, installed sysconfig_1.17.0, Updated IAR to IAR EW for Arm 9.40.1
Following instructions, i was able to copy and create example project in new directory, but still cannot…
Hi Xiaodong Li, I was reluctant to follow your hint, because I've already tried with TI Uniflash. But yes indeed, the current version of CCS was able to update the debugger. After that, I retried with IAR V8.1 and now it is able to use this debugger…
Thank you Kritsnam. I am waiting to get approved for an IAR license to replicate the issue. I've been able to test the program with IAR Workbench version 8.20 and did not have the issues you are seeing.
Let me know if you have any new findings. I…
Part Number: IAR-UPDATE Other Parts Discussed in Thread: CCSTUDIO Good Morning everybody!
This morning, while I was trying to do the debug of my Code in ASSEMBLY with the IAR, the compiler shows me this message:
"Your code is too large. This IAR version…
Of course, thanks for making the update.
Can you verify that you are using the MSPM0G3507 Launchpad, as opposed to another MSPM0G device such as the MSPM0G3506? Additionally, could you specify which version of code composer studio you are using?
The default…