Part Number: LAUNCHCC3220MODASF
Hi TI, We are currently using CC3220MODASF and need to configure additional parameters (cloud device name and secret key) in addition to WiFi SSID and password. Can you recommend a method for this setup?
Hi noushadali k , Is this thread in relation to the same question: https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1341257/launchcc3220modasf-challenges-in-integrating-ble-and-gsm-functionalities-on-ti-cc3220modasf-launch…
Part Number: LAUNCHCC3220MODASF Hello all,
I want to verify the data written at the OTA update using the TI example out_of_the_box\ota_archive.c . The answer in the topic e2e.ti.com/.../cc3235modasf-sl_fswrite---data-consistency inspired me to simply add…
Hi,
No. You can't have two masters at one SPI bus. One device need to be master other device need to be slave. Slave input need to be connected to master output. Master input need to be connected to slave output.
Jan
Part Number: LAUNCHCC3220MODASF Other Parts Discussed in Thread: CC3220SF Hello,
Using CC3220MODASF, I faced an error building the cloud_ota app as it couldn't find "ota.a" library at ti/net/ota/ccs/Release/ota.a path. SDK check revealed the missing ota…
Hello TI, E2E community,
I am currently working on a project where I need to establish communication between an MCU (specifically the CC3220 Launchpad) and a GSM modem using AT commands via UART. Furthermore, I aim to establish network communication…
Part Number: LAUNCHCC3220MODASF Hi, We are currently working on the cc3220MODASF launchpad. I attempted to run the adsignalchannel sample code following the instructions in the readme file, but I am unable to properly read the ADC. The output is attached…
Part Number: LAUNCHCC3220MODASF Hello everyone,
where can I set in CCS whether the project uses RAM-Based Peripheral Driver Library or ROM-Based Peripheral Driver Library? The manual CC32xx ROM services mentions the global preprocessor define USE_CC3220_ROM_DRV_API…
Part Number: LAUNCHCC3220MODASF Other Parts Discussed in Thread: SYSCONFIG Hello I am using LAUNCH3220MODASF launchpad and ccs version 12.0. When I trying to build mqtt_client example get following errors . I am importing mqtt_clientexample code via…