Part Number: LAUNCHXL-F28027F Other Parts Discussed in Thread: LAUNCHXL-F28027 , C2000WARE The problem statement can be accessed from here . Further, the code (CCS) is #include "F2802x_Device.h"
#include "f2802x_examples.h"
#include "f2802x_epwm_defines…
Part Number: LAUNCHXL-F28027F Other Parts Discussed in Thread: DRV8323 Hi, I am using the DRV8323 as a motor driver alongside the F28027f to drive this motor ( https://store.tmotor.com/goods-856-RI50+KV100.html ). I've followed the setup guide that is provided…
Part Number: LAUNCHXL-F28027F Other Parts Discussed in Thread: MOTORWARE , DRV8323 Hello, I am running a BLDC motor. The control is sensorless. If the motor is now driven to a stop so that it can not rotate further, the motor makes a knocking noise and jerks…
Part Number: LAUNCHXL-F28027F Hello, Everyone.
I just wondering, where i should connect the QEP sensor from the motor Teknic 2310P using LaunchpadXL F28027F, i just cant find that pin on the microcontroller board. What the J3 for?
Thanks in advance,
…
Part Number: LAUNCHXL-F28027F Other Parts Discussed in Thread: MOTORWARE I am new to the c2000 family and recently tries to utilize the HRPWM module to get Duty cycle of 50.3% at 500KHz switching frequency with the clock seed set to 60MHz. Below is the…
Part Number: LAUNCHXL-F28027F Other Parts Discussed in Thread: DRV8353 , ISO7740 , C2000WARE-MOTORCONTROL-SDK , DRV8353R , TMDSEMU110-U Hi Experts,
Our customer wants custom LAUNCHXL-F28027F for control DRV8353, but ICs ISO7240 and ISO7232 are out of stock…
Part Number: LAUNCHXL-F28027F Other Parts Discussed in Thread: DRV8305 , MOTORWARE Hello sir,
I am using LUNCHXL F28027F + DRV8305 for controlling BLDC Motor. Speed of motor varies from 900 to 8000. But motor doesn't stop immediately. Is there any brake…
Hello,
My apologies, but I do not understand what you are looking for.
GuCheol Jeong said: Now I'm trying to use the encoder and motor using F28069M MCU but the all header files are different.
This what I am not clear on.
Part Number: LAUNCHXL-F28027F Other Parts Discussed in Thread: C2000WARE-MOTORCONTROL-SDK , C2000WARE , MOTORWARE
Hi,
I want to use sensored FOC control on LAUNCHXL-F28027F for PMSM motor control.
Is there any example code for sensored FOC control that…
Part Number: BOOSTXL-DRV8323RH Other Parts Discussed in Thread: LAUNCHXL-F28027F , , MOTORWARE , DRV8305 , DRV8323 I wish to use the hardware controlled version ie: BOOSTXL-DRV8323RH paired with a LAUNCHXL-F28027F Launchpad. The doc below indicates that this…