Part Number: TPS7A96 Other Parts Discussed in Thread: TPS7A57 , TPS7A47 , TPS7A3501 Hi Team,
I have a customer who have a question on cascading LDO.
Assuming that we have a cascaded power supply tree 24V-6-5-3.3 where the last 2 stages are LDO, customer…
Part Number: LP2992
Hi,
We have tested a circuit that takes a 10s cell pack which idles at 42V full charge and is connected to a LV2862Y dc dc converter to make 12V from the cells. We also have an LDO at the 12V which generates 5V and is connected to…
Part Number: TPS7H5001-SP Other Parts Discussed in Thread: TPS7H5005-SEP The application in question utilizes a power bus with maximum operational voltage of 33.8V and must be radiation tolerant (unfortunately this rules out the TPSH4010-SEP). My question…
Part Number: TLV773 Other Parts Discussed in Thread: TLV759P , TPS746 Hi team,
could you help to see below request? do we have recommendation for a low cost LDO?
Project: Smart door lock Selection requirements: 1. Power supply voltage: the minimum input…
Hi Nick
The DC fan is the only load for the LDO. The current of fan is 130mA. The waveform is AC coupling of LDO's input side when fan was running. The output of LDO @ fan was running has similar ripples. Thank you.
Rong
Part Number: TPS65994AD Other Parts Discussed in Thread: TPS65992DBH , TPD6S300 Hi,
For TPS65992DBH, what is the LDO current ability?
Could we use it to provide TPD6S300 3.3V power?
Thanks!
Jeff
Part Number: BQ24617 Dear Sir,
I am currently working on a new project that involves utilizing the BQ24617 for the pilot. However, I have encountered an issue where the quiescent current exceeds the specified 2mA mentioned in the datasheet. Upon further…
Part Number: LM5148 Hello,
The LM5148 datasheet specifies that both VCC and VDDA can be used as LDO in the system, and that VCC is connected to PGND while VDDA is connected to AGND.
Can either VCC or VDDA supplies be used used to power other portions…
Part Number: TPS7A20 Dear Team,
I am using below LDO in my design.
Can you suggest an alternate P/N.
https://www.digikey.in/en/products/detail/microchip-technology/MCP1727T-3302E-MF/1098497?s=N4IgTCBcDaILYGMAOBGA7GNAXAtAZjwAYwBTAejgDMQBdAXyA
https:…
Part Number: TPS717 Hello I am using the TPS71750DSER LDO regulator in a PCB design. I am trying to simulate the noise at the output in LTSPICE simulations.
Does the model file for the part, "TPS71750_TRANS.lib" properly incorporate the noise into the…