Hi Travis,
we chose the TPS53632-LMG5200POLEVM-10 EVM since it seemed to be good for a proof of concept for our laser diode driver and it was the only reference-design available for our specs. We do not have any experience with isolated power-conversion…
Part Number: LMG5200POLEVM-10 Other Parts Discussed in Thread: LMG5200 Hello,
can you tell me the reason behind leaving exposed copper areas in the reference design TIDUC72A that is using the LMG5200.
See link: https://www.ti.com/lit/ug/tiduc72a/tiduc72a…
Part Number: LMG5200POLEVM-10 Other Parts Discussed in Thread: TPS53632G Hi,
I am looking for the best method to program LMG5200POLEVM-10 from my computer. What USB adapter and GUI do you recommend? Is there any additional software needed to communicate…
Part Number: LMG5200POLEVM-10 The User Manual of the EVM explains:
The converter topology and transformer turns ratio (5:1) restricts the maximum output voltage to be 1/20th of the input voltage.
In that manual, there are two windings visible in the top…
Hi Matthew,
I should have been more descriptive in my previous post. The TI design I mentioned in my previous post for which I have shared the URL below is for analog Hysteresis control. My precise requirement is whether TI has any reference code for hysteresis…
Hello Danilo,
For buck converter application, the LMG5200 EVM could be a good starting point. https://www.ti.com/tool/LMG5200EVM-02
For such a low output voltage, some topologies such as half bridge with current doubler can be considered.
We have a reference…
Sure,
LMG5200POLEVM-10 with SV601229 Rev. B board Design Files. It has the complete Altium Project, to help fast prototype with verified solutions for noise integrity etc. Meanwhile, usually only .OutJob files are included which can only generate .PDF…
Hello Stefan,
Yes, LMG5200 EVM and BOOST-3PhGaNInv should get you familiar with GAN. GaN FET has many advantages over Si MOSFET like zero reverse recovery, which allows using GAN FETs in half-bridge configuration, much less output and gate charge losses…
Part Number: UCC27511 Other Parts Discussed in Thread: UCC27611 , LMG5200 , LMG5200POLEVM-10 Hi,
UCC27511 is a low side MOSFET driver, I would like to know if there is any evaluation kit using this part so that I can test it to see if the performance satisfy…
Hello Rizwan,
What is your input voltage? 1V 1000A at the output requires very low Rdson FETs. However, LMG5200 can be feasible for the primary side. If the input voltage, for instance, is 48V, 1kW corresponds to a current of about 20A at the primary…