Part Number: LMK04828BEVM Other Parts Discussed in Thread: USB2ANY Hi
For this development board, we downloaded the TICS Pro software, chose the LMK04828B chip, plugged in the connector, and connected the computer to the development board, but the connection…
Part Number: LMK04828BEVM Hi,
Just a quick recap for this question. Can You send again this file with the newest version of the pllainumsim because it seems when i load the file i cannot open because it was created with a previous verion or alternatevily…
Part Number: LMK04828BEVM
I am designing clock file LMK04828B for RFSOC4x2 board, with SLKin 100 Mhz, External VCO 160, and VCO/Clock Dist. Frequency 3000 Mhz. PLL1 and PLL2 are not locking.
cliff_try (2).tcs I am attaching a .tcs file as well in the…
Part Number: LMK04828BEVM dear Ti team,
i am using the LMK eval board- LMK04828BEVM which is working fine with internal clock 122.88Mhz, but my requirement is need to provided an external clock of 60Mhz as in put to the LMK and generate 800Mhz and 100Mhz…
Part Number: LMK04828BEVM Other Parts Discussed in Thread: LMK04828 Dear TI Team ,
I am evaluating the LMK04828BEVM board, my problem is that I need to know the settings needed to be done in the SYNC/SYSREF to generate square pulses.
With…
Part Number: LMK04828BEVM Other Parts Discussed in Thread: LMX2572 , LMK04828 We are working with a LMK04828B board and TICSpro
We are trying to generate a 1 GHz clock using a 25 MHz input (CLKin1).
1. In our first configuration we use an AWG to generate…
Part Number: LMK04828BEVM
I configured it with evkit as shown in the picture below.
After setting pulse mode using clk0 port, SDclkout outputs undesirable signal in signal standby state.
If the LVDS signal of the FPGA EVKIT is separated, it is output…
Part Number: LMK04828BEVM Other Parts Discussed in Thread: AFE7906 , LMK04828 I have AFE7906 ADC , need to give device clock and Sysref for ADC and FPGA from LMK04828 ,can we connect both OSCin and clkin pins
Part Number: LMK04828BEVM Hi.
The only way that I found to check if the PLLs are locked is to check the Status_LD1/2 pins.
Is there a way to check if the PLLs are locked from the registers interface?
Thanks,
Almog.