Hey Vincente,
We don't have a local FAE or a field office. So, we are thinking of buying a new LMX2595EVM. Can you recommend some good practices so that we can operate the EVM safely and avoid such problems again?
Also, can you help us with some good…
Part Number: LMX2595 Hi
We use LMX2595, but we cannot control the output of 5G. Currently, we need it to output a clock of 5G
And can not be observed with high-end oscilloscope, according to the datasheet description process operation: configuration…
Part Number: LMX2595EVM Other Parts Discussed in Thread: LMX2595 , , LMK61PD0A2 Hello, I observed a phenomenon that puzzled me.
When my LMX2595's reference signal is set to 125MHz, no matter what output frequency is, there is always a 3.5GHz spurious output…
Part Number: LMX2595EVM Other Parts Discussed in Thread: LMX2595 , LMK61PD0A2 , LMX2485E
Hello Sir,
We plan to use two PLL to generate an 12.8GHz LO.
Use SYN1 to generate the 100 MHz , use the SNY2(LMX2595) (with the 100MHz reference)to generate a final…
Part Number: LMX2595EVM Hello,
We are testing the LMX2595EVM and notice these spurs across a huge spectrum. They seem to be PFD spurs (not sure).
However what do we do get rid of them (right from <1GHz to several GHz).
Following are the spectrum…
Part Number: LMX2595EVM Other Parts Discussed in Thread: LMX2595 In LMX2995EVM we can install a 100 MHz crystal oscillator at Y1. Can you give the manufacturer part number of recommended oscillator.
Regards,
Amit
Part Number: LMX2595EVM Other Parts Discussed in Thread: LMX2595 , USB2ANY Hi There, I bought the LMX2595EVM to use it as an RF Synthesizer locked to an external 100MHz. However, I can only measure -0.5dBm at the RFOutAP (RFOutAM is 50Ohms to gnd and RFOutB…
Part Number: LMX2595EVM Other Parts Discussed in Thread: LMX2595 Hello. We are testing the LMX2595EVM with two 100MHz OCXOs. The frequency of reference clock is 100 MHz and Osc_doubler of LMX2595EVM is enabled.
We found that when the LMX2595 is in integer…