Part Number: MDL-BDC Hi guys,
I'm Toan. A few weeks later, i bought a RDK-BDC24 to research and study. But in GUI i cant excute CAN. So i try to update firmware in boot_can folder. And you know, my device seem be died, no led flashing, cant update firmware…
Good Evening,
Recently, we have attempted to update our MDL-BDC24 Black Jaguar to firmware v101 (http://www.ti.com/litv/zip/spmc014b) (to support CAN). We downloaded BDC-COMM from the ti/jaguar website, and connected it to the left rj12 adapter. Upon…
I am using EVE SW version "eve_sw_01_18_00_00" .
my testcases passes with the image. please find attached input image. PLEASE REMOVE THE .txt EXTENSION BEFORE USING THE IMAGES. I CHANGE THE EXTENSION TO UPLOAD THE FILE BECAUSE FILE IS NOT GETTING…
Hi Margaritha,
What could be the reason that mdiscalar and hdiscalar elements behaving differently?
One thing I observed that while using mdiscalar element 2 out of 3 frames capturd are full of grains as shown in the snapshot below
yuv file : (convert…
Hi Praveen,
I referred the section 3.6.5, optimized frozen graphs for MobileNet and tried to run the generated .pb but it's also showing error in tidl_log.txt file as :
"
TF Model File : ..\..\test\testvecs\config\tensorflow_models\mobilenet…
Hi Vivek,
I have C6000 Labs and Solutions. I'm not sure if they were meant for the OMAPL138 or not. The comments in the code say '6748 EVM'. I will post them so you can have a look.
Best regards,
Janet
2477.TI_RTOS_Labs_and_Sols_C6000.zip…