Part Number: MMWAVE-STUDIO Other Parts Discussed in Thread: IWR6843AOPEVM , IWR6843AOP , MMWAVEICBOOST I was following DCA1000 quick start to install mmWave-studio, 2.0. After I installed mmWave-studio, it can start, however, I didn't see XDS110 class…
Hello Anirban,
I have no idea why mmWave Studio didn't run... But I feel that the operation of DCA1000 is unstable.
By the way, I think it would be better to change ”SOP2” to other name.
Since "SOP2 mode" and "SOP2 switch" exist in your mmWave…
Part Number: TIDEP-01012 Other Parts Discussed in Thread: AWR1243 Hello,
I am using TIDEP-01012. It was working fine yesterday but the device is showing some error issue.
here is the log that i got from mmwave studio.
[15:36:58] RstdNet: Port 2777: Client…
Part Number: AWR6843AOP Hi Ti, According to my understanding, using mmWave studio, the signal can be changed to CW mode for operation, and more subtle AOP information can be obtained. I have the following two questions: 1. Can I only use it through DCA1000…
Hi Parjanya,
Parjanya Yaragani said: when im trying to run the mm-Wave Demo visualizer it keeps showing this:
Are you running the SDK demo? Do you want to capture ADC data while running the demo? If yes, you can try using Studio CLI tool present in t…
Abhishek,
Thank you for the quick reply. I appreciate you looking into my issue. For reference, the mmWave Studio guide version I followed is this one:
DCA1000EVM mmWave Studio Guide
Thanks again. I'll keep an eye out for your response.
Have a great…
Part Number: AWRL1432BOOST Hi,
I want to config slow-fast frame using mmwave studio4.1.0.5, what should i do?
TRANSLATE with x
English
Arabic
Hebrew
Polish
Bulgarian
Hindi
Portuguese
Catalan
Hmong Daw
Romanian
Chinese Simplified
Hunga…
Part Number: IWR1443BOOST
Hello TI team,
I'm capturing the data using mmWave studio continuous streaming tab and I'm processing the captured data by writing my own code, but from the mmwave interface I'm not getting the exact idea about the following…
Part Number: MMWAVE-STUDIO hi,
I have a confusion that when I download the two pre-built bin image to radar device using mmwaveStudio, how can I choose one mode between USRR and MRR in mmwaveStudio?
whether it means that I need to modify FMCW Bandwidth…
Part Number: MMWAVE-STUDIO Looking into swra555a and swra581b I'm still a little confused regarding the format of the LVDS data transferring, using DCA1000:
1. IQ Swap - I first means I is in LSB, i.e. comes to lower adresses in the buffer than Q…