Part Number: MSP-CAPT-FR2633 I have an older eval kit of the MSP-CAPT-FR2633 that came with the CAPTIVATE-PROMITY Rev B board. I could not find any example files for it, and upon further research I found it was discontinued.
If possible I would still…
Part Number: MSP-CAPT-FR2633 Hi,
MSP-CAPT-FR2633 is indicated "not available" on your web site.
( http://www.ti.com/tool/msp-capt-fr2633
Do you have way to order?
Best regards, RY
Part Number: MSP-CAPT-FR2633 MSP Captivate Devices used for testing: 1) Captivate Programmer Rev C 2) Captivate FR2633 Rev C 3) Captivate BSWP Rev B 4) Micro usb cable arrived in Box.
System Environment: 1) Operating System: Ubuntu 16.04 LTS (64 bit, x86_64…
Part Number: MSP430FR2633 I tested low power consumption with MSP-CAPT-FR2633 Development Kit ,and the development board used the default software.
When the standby power is adjusted from 3.0V to 2.0, the standby power consumption can reach about 3UA…
Part Number: MSP-CAPT-FR2633 Tool/software: Code Composer Studio Hi,
I am trying to install CC7.4 and it is failing because the software is unble to find a windows update patch KB3033929.
When I try to install the patch, my computer says it is already…
Part Number: MSP-CAPT-FR2633 Tool/software: Code Composer Studio Hi,
Before I describe my problem, I will explain how I got there. I am developing a product that requires capacitive touch. I have generated code from the captivate design center to trigger…
Part Number: MSP430FR2633 Other Parts Discussed in Thread: MSP430F5529 , MSP-FET , Should we able to SW invoke I2C BSL with MSP-CAPT-FR2633?
HW invoke seems to work fine https://e2e.ti.com/support/microcontrollers/msp430/f/166/t/599242
(though how are they…
Part Number: MSP-CAPT-FR2633
Tool/software: Code Composer Studio
Hi,
I need help to configure this board to read mutual capacitance between two copper electrodes. I need to get the raw value to change a display based on that. Please advice which tutorial…
Part Number: MSP-CAPT-FR2633
Hi there!
I'm trying to understand the total sensor conversion time calculation.
When I click help in the Design Center GUI under Scan Time Estimate tab of the controller properties, it says " As shown in the formula…
Part Number: MSP-CAPT-FR2633 hi all,
a customer of mine has developed a touch keyboard w/ our captivate technology...
he is asking whether (and if yes, how) is possible to detect multiple keys pressed at the same time (or if there will be a dominant one…