Part Number: MSP-EXP430G2 Hello Team,
Posting on behalf of my customer:
I have a launchpad MSP-EXP430G2 with an MSP430G2553 and I want to run code from my mac book pro wich has a M1 Pro chip. I tried downloading CCS but the program doesnt recongize that…
Part Number: MSP-EXP430G2 After puzzling over this off and on for the last couple of weeks, reading tens of E2E threads I can't seem to find a solution. I suspect that because I first used CCS with the MSP430 USB Debug Interface (MSP-FET 430UIF) that…
Part Number: MSP-EXP430G2 Trying to get I2C transmission working on a MSP-EXP430G2. The desire is to have SMCLK connected to SCL at ~100khz. I have a logic analyzer connected to SDA and SCL with 4.7k external pullups connected. At startup both signals…
Part Number: MSP-EXP430G2
Hi Team,
Following Section 2.3.1 of the SNLU197 USB-2-MDIO Software Tool user's guide, our customer encountered an error when he ran the Flash_MSP430_F5.bat file as shown in the screenshot below. I searched for similar error…
Part Number: MSP-EXP430G2 Is the MSP430 LaunchPad (MSP-EXP430G2) compatible with version 5.1.0.09000 of Code Composer Studio. Can I run it on the newer launchpads?
Part Number: MSP-EXP430G2 Hello!
I have a MSP-EXP430G2 Launchpad board (eZ430) and it stopped working.
It was without use during about 1 year and when I tried to use now and connected the cable in PC, the board was not recognized and is not enumerated…
Hi Evan,
Many thanks for the kind and prompt support. Point wise replies below:
Using CCS v6.1.1 on Win8
Create new CCS project, select MSP430G2553
Opt for demo LED example
Build All
Launchpad "MSP-EXP430G2" connected and detected on Mini USB cable…
Other Parts Discussed in Thread: BOOST-DRV8711 , MSP-EXP430G2ET hi
I have a problem with the cards (MSP-EXP430G2ET + BOOST-DRV8711) I cannot use BOOST-DRV8711_GUIv1.0
see photo
Part Number: MSP-EXP430G2 I am attempting to program the MSP430FR2675 by using the MSP-EXP430G2 launch pad, I was told since both have SBW I should be able to accomplish this by hooking up the RST, VCC, VSS, and TEST pins from the launchpad to the FR2675…