Other Parts Discussed in Thread: MSP430F6438 Hi,
I just bought a MSP-FET430U100C and insert the 6438 chip into it.
Right now the laptop can recolonize the device, but when I try to load the code into the chip, the code composer V5 shows Unknown device…
Other Parts Discussed in Thread: SYSBIOS , MSP430F6438 Hello,
i have bought an MSP-FET430U100C Evalkit and there will be two MSP430F6438iPN Controller which are equiped with everything i need. I was searching fo the fastest way to get a RTOS running. So…
Hello,
first: i have posted this yesterday in the MSP430 forum but no one gave a reply.
i have bought an MSP-FET430U100C Evalkit and there will be two MSP430F6438iPN Controller which are equiped with everything i need. I was searching fo the fastest…
Other Parts Discussed in Thread: MSP-TS430PZ100 Hi,
I can't find the schematic diagram for the MSP-TS430PC100C target board on the CD that came with my order for MSP-FET430U100C. I did find the '100B schematic and layout, but that looks different since…
Lisa:
I have good news to report. I have now installed CCSv5.5 on both my Windows 7 desktop and my Windows 8 laptop. In both cases I did run the setup as Administrator. That was the key, apparently, in Windows 7, and I didn't bother to check if it wasn…
I would make a recommendation in this order:
1. MSP430FR5969 in RGZ package with MSP-FET430U48C socket board 2. MSP430F5335 in PZ package with MSP-FET430U100C socket board 3. MSP-EXP430F5438
On the MSP430FR5969 you can use the FRAM memory as data memory…
Hello David,
The MSP430 line of MCUs have JTAG interfaces. This is similar to the BDM interface used by P&E debuggers. You can do all the hardware debugging in real time along with single stepping And emulation
The stand alone feature of the Cyclone…
I didn't notice that the pins weren't compatible there. I will get the MSP-FET430U100C when I get a chance. Strangely, everything seems to work fine.
I realized my simple mistake was that I had my oscilloscope on AC coupling instead of DC coupling…
Howard Tang said:
I need to buy a MSP430 and it will be mounted on PCB with my power management unit, which type of packaging should I buy?
You will need to select the ideal MSP430 for your application based on your requirements. You will know these…