Part Number: OMAP5432-EVM Tool/software: Linux Dear Sir/madam;
We had purchase the "omap5-uevm" board to test the ov5640 5MP camera sensor on CSI-2 [MIPI] interface. We follow the " http://processors.wiki.ti.com/index.php/OMAP5_GLSDK_S…
Part Number: OMAP5432-EVM Tool/software: Linux HI,
Can anyone help me figure out the exact problem. I am unable to boot linux on omap5432-evm board. The kernel I am using is 3.8.13. Following is the console output as well as the device tree. Thanks
[…
Part Number: OMAP5432-EVM Tool/software: Linux Hello, Can anyone help me with this issue. I am trying to boot linux 3.8 on OMAP5432-EVM platform but i get the following message. I am also attaching the device tree. Thanks
3.312500] [drm] Initialized drm…
Part Number: OMAP5432-EVM Hi,
I had a chat with someone in support and they sent me here. I'd like to request the IBIS models for the OMAP5432 and TWL6037.
Thanks
Part Number: OMAP5432-EVM Hello,
I am currently reading the BSDL file for the OMAP5432 and have a few questions:
what does "IOType" mean?
What is IOType used for?
Where can I find information on the IOtype programming for JTAG for the OMPA5432…
Part Number: OMAP5432-EVM-EVAL-SW hello
i have i eval board in our school lab. i am new at ti dsp. our kit has omap 5912zzg chip. one ti expert said me it has no internal flash when you write a code it save it to external(nor or nand) flash memory. but…
Part Number: OMAP5432-EVM Tool/software: Linux Dear All,
i am using OMAP5432 and i need to boot by using SD card firstly what will be the Switch Configuration and when i am running cmd mksdboot.sh to boot SD Card with In=mage and File system i am getting…
Part Number: OMAP5432-EVM Tool/software: Linux WiLink experts,
Greetings! I am in search of a WiLink module and corresponding SW to interface to both the WLSDIO3 and SDIO4 modules on OMAP5432-EVM. The goal is to validate read/write access on the units…
Part Number: OMAP5432-EVM
Tool/software: Linux
Hello everyone, We are using the " platform_device_register(&omap4iss_device )" function call to add the platform data for the oma4iss driver. where the omap4iss_device structure is as below. static…
Part Number: OMAP5432-EVM Tool/software: Linux Dear all,
i downloaded Android pre build image and i am using UBUNTU 14 as host system i want to know how to boot image file into its emmc
i configured booting switches to 0000
and connected USB3 to my h…