Hi Ben,
Regarding reference design PMP40281, I am looking for the EVM BOARD that works with the converter Controller Card, UCC256302.
Trying to review the schematic for PMP40281 and J1. What EVM board works with the Converter Controller Card.
This Controller…
Part Number: LM5021 Other Parts Discussed in Thread: PMP10215 , , PMP40281 , UCC256402 Hi, TI expert,
Currently need to make a two-tube forward design with 300~1000V input Voltage, 24V output Voltage and 200W output Power.
Suppose LM5021 is the suitable…
Hello Ram,
Please see TI Home > TI reference designs search This is where ALL of TI reference designs are located.
In the search PARAMETER window enter; Vin min 230V, Vin max 260V, Select AC input, Vout 24V, Iout 12A, http://www.ti.com/reference-designs…