Part Number: PMP4844 Hi,
Our input requirement is 16VDC-48VDC and output is 24VDC/5A .
Can we able to implement the PMP4844 reference design.
If it is possible can you please provide the design details(like Resistor, Capacitor Formula and calculation) …
Part Number: PMP4844 Tool/software: WEBENCH® Design Tools I am referring to reference design PMP4844
Please share transformer details for manufacturing transformer. Transformer part no.mentioned in BOM is G095024LF, but this part no. datasheet do not mention…
Part Number: PMP4844 Hi,
We are going to use PMP4844 design
Our input range: 20VDC to 32VDC
Output:24V@5A
What are all the changes need to be done for our input range.
Part Number: PMP5123 Other Parts Discussed in Thread: PMP10861 Hello Team,
one of our customer is planing to build a PMP5123 and PMP4844.
--> Do you have a datasheet availble for?
PA4138NL (T1 in PMP10861 and PMP5123), Pulse Engineering Transformer…
Part Number: UCC2897A Other Parts Discussed in Thread: TPS28225 Hi,
We are going to use PMP4844 design for our power requirement Vin 20-32V vout:24V Iout:5A.
In PMP4844 control driven rectification is used.
I am calculated the sync rectifier's power loss…
Hello Sir,
by twice the output voltage you got twice the output power, here 72W; would recommend to go from a flyback to an Active Clamp Forward topology. Better efficiency, less EMI and well suited for power range 50W to 150W.
Please check UCC2897A or…
Hi Harry,
So sorry for the trouble here, I mistyped the design number, so that transformer from GCI is actually for PMP4844, not PMP4484 that you asked about.
The correct part is the one that you referenced from the previous thread. Again, sorry for my…
Hi Masazumi-san,
Thanks for your interest in UCC256304. UCC256304 must be able to charge up its VCC pin to 26V before switching begins. I would advise against using this controller if the input range is 14V to 36V.
If I may suggest an alternative,…