Part Number: PMP5651 Hi,
I am looking for Flyback DC-DC converter with 50V@1.4A Output.
This PMP5651 design is suitable for my requirement. Someone please provide me the design files of this reference design.
regards
Naresh
Part Number: TPS40210 Hi Sri,
Our customer want to use the TI PMP5651 ref design, but have some question. Could you please Description?
Q1 Waht's the R200&Q201&D200 function? Clamp voltage to protection TL103? Q2 what's the D6 MMSD914 job function…
Hello Neelesh,
The prototype of PMP5651 has been built using the PCB from PMP4963. I attached the Gerber data and the assembly drawing accordingly.
Best regards,
Roberto PMP4963_REVC Gerber.zip PMP4963_REVC_PCB.pdf
I'm looking for a solution similar to PMP5651. 22V-50V input, 53V-54V output, but with a higher output current requirement of 2.5A.
It would look like that major changes would be 63V or higher rated input caps, transformer and rectifying diode with…