Hello,
Could someone advise me how to modify PMP5732(100-277VAC Input, 25-36VDC, 1.5A Output) reference design
to supply 33-39VDC, 1A Output?
Thanks in advance,
Yesok Yoon
Other Parts Discussed in Thread: UCC28810 Hello,
I am looking for the spec and design tool for the transformer(UCC28810 FB) of PMP5732(100-277VAC input, 25-36VDC, 1.5A output) reference design.
PMP5732 is based on PMP5560(180-264VAC input, 12-25VDC, 2A…
Other Parts Discussed in Thread: UCC28810 Hello,
I want to modify output voltage range of PMP5732 from 25-36VDC to 33-39VDC.
Could someone tell me the factors affecting output voltage range of UCC28810 based LED Driver so that I may finish my project? …
Dear All,
I am using PMP5732 -36V @ 1.5A solution for LED Driver.
In that current harmonics are 27%.
Please help us for reducing the current harmonics to less than 15%
Hai,
I am using PMP5732 design for our 48led driver - 40V @ 1.4A. The pcb designed and starts testing after populating the components.
Issues: 1. No load wattage is around 4.5W, 2. Output voltage is increasing beyond 85V.
Please helps us for sorting out…