Sergiu,
Referring to section 6.10.1.5 Troubleshooting Motor Shaft Stopping During Ramp-Up of the InstaSPIN User's Guide, the guide states that "The motor shaft needs to start moving at all times during the ramp-up process." Later in 6.10.1.8, the guide…
Part Number: TMS320F28069 I've been working with custom hardware to try to identify a compressor.
The bus voltage is 48V on a 25A power supply.
I've checked the calculations for my hardware a few times, but here's my user.h file.
5482.user…
Part Number: TPS61177A I have a design with TPS61177a, following the reference design.
there's another device on i2C bus with address '5d'.
after asserting the 'ENB' pin, I can find two devices on I2C line with address '2C' and '5d'.…
Part Number: BQ76952 TI experts,
14S of 30Ah battery, 60A (2C) discharge, CUV setting is 2.83V, but no CUV protection occurs until 2.4V is discharged.
The battery samples are about to be shipped to customers. Can you help me see what the problem is…
Part Number: BQ28Z610-R1 Hi Team,
Could you explain more detial about the new features of BQ28Z610-R1 "Bus low timeout reset of the I 2C engine"?
Is that mean timeout will keep counting if there is no communication action?
Thanks and best regards…
Part Number: TMS320F28054F Tool/software: Code Composer Studio After identifying our low inductance PMSM motor controlled by a custom board, we tried to run the motor in the second part of lab 2c and it was choppy. We were able to get a good waveform…
Part Number: TDA2EG-17 According to the picture below:
I want to send some data to「Slave」by I2C. Now, it's no problem to send data to「DES」and「SER」, but I can't send data to「Slave」by I2C successfully.
I have set「Slave ID」(0x08) and「Slave Alias…