HI Francesc,
Can you send me the full installation path to your Sensor Controller Studio install folder ?
Also, other steps you may try: _ In the Windows Registry Editor, can you delete the following folder under:
_ Can you post the content of the .osd…
Part Number: SENSOR-CONTROLLER-STUDIO
Sensor Controller Studio is used to write, test and debug code for the CC26xx/CC13xx Sensor Controller, enabling ultra-low power application design. The tool generates an interface driver consisting of C source files…
Hi Manuel,
In that case, I think you could indeed use COMPA, coupled with the TDC to get the time, as if you would do for capacitive sensing.
Only this time, you would actually monitor the capacitor discharge.
Here is it, described in the Sensor Controller…
Part Number: CC1312R Hi,
I have a sensor controller task that waits for ADC readings to stabilize. It is an auto-calibration application repeated for 6 input settings controlled by an analogue switch via SPI.. The whole process can take up to 20 seconds…
Part Number: DRV8353RH-EVM Hello Team,
we want to order DRV8353RH-EVM evaluation kit for out testing purpose. As per brief description (snapshot below) it is written it is ideal for sensorless control. can we driver motor in sensored mode by using our…
Part Number: TMS320F28069M Other Parts Discussed in Thread: MOTORWARE , It seems like in Motorware, the sensored speed and position control example projects use encoder for position and speed feedback. Are there any example projects that apply Hall sensors…
Part Number: LAUNCHXL-CC1352R1 Other Parts Discussed in Thread: MSP430FR2433 , CC1352R Dear Experts,
Currently, i have developing the smart meter device with cc1352R1 and MSP430fr2433, this device consumes 200uA to 300uA during sleep(60min), i have used…
Part Number: CC2674R10 Other Parts Discussed in Thread: CC2652R7 , CC1354R10 * Context: on our custom PCB, we have unsoldered CC2652R7 and soldered CC2674R10 in place. Our plan is to update the software *without* modifying the hardware. We are using s…
Part Number: TMS320F280049C Hi community,
So right now I'm driving a BLDC motor using DRV8320RS(Driver Board).
This Driver board produces 3 phases as output from it which will be input in BLDC motor for driving it.
So after driving it now I've to…
Part Number: CC2652R Other Parts Discussed in Thread: SYSCONFIG Hi,
I'm using the sensor controller to make ADC measurments in 16 kHz, I'm using timer 0 in the sensor controller to control the timing of these measurements. The data is then reported over…