Part Number: TIDA-00056 Hello! Is there a complete list of gases available? Written in this document are carbon monoxide, oxygen, ammonia, fluorine, hydrogen sulfide, and "others". A customer is inquiring if Ethylene Gas is included. Thanks!
Part Number: CC2541 Tool/software: Code Composer Studio Hi Team, This is a customer request I would be happy if you can help.
"
For our new project we decided to use TI Gas detector reference design.
The software is on IAR but we use CCS, Can you…
Part Number: TIDA-00056
Hi,
I am using Gas Sensor Platform with Bluetooth Low Energy (LMP91000 with CC2541). I found a project called SensorBLEPeripheral that supports both CO and O2 sensors. My problem is that I couldn't change Vbias value using the existing…
Part Number: TIDA-00056 I am using the reference design for electrochemical gas sensors. My question is related to temperature logging in the iPhone app "TI gas sensor".
Is possible to export the temperature data in addition to the current and…
Need help on how to develop complete solution (device) to monitor Ammonia gas (NH3) in the confined space, i.e. restroom.
I am interested in using TIDA-00056 with its BLE to transmit data to app. Do I need to have other TI's components/devices to build…
Part Number: TIDA-00756
Tool/software: Webench
Hello,
It is sorry to type PN:TIDA-00756. Because TIDA-00056 is not recongnized. I learn Gas Sensor Platform Reference Design TIDA-00056 and have some confusions in my mind.
Could you please help to answer…
Ajinder,
I'm sorry to say that I am at my wits end. for the life of me I cannot understand what I'm doing wrong however when I put the sensor in testing I cannot get a reading on any H2S. Are there limitations to the TIDA-00056? the sensor I…
Dear Gordon,
I was able to find a sutable configurations for the sensor, however, it seems that I require the TIDA-00056 Gas Sensor Firmware, the datasheet only shows how to configure it using the "IAR Embedded Workbench" which is quite expensive,…
Dear Amir -
Yes, if the sensor is a two or three leaded electrochemical sensor -it should support it.
Here is a compact design example in case you did not come across it yet.
https://www.ti.com/tool/TIDA-00056
Hi Josh,
Thank you very much for your reply.
I am applying the settings that LMP91000 GUI suggested. But I am confused. It does not tell me to set the sensor as two wire mode. Please refer the screenshots I have attached.
This is from the GUI.
This…