Part Number: TIDA-00499 Other Parts Discussed in Thread: BQSTUDIO , , EV2400 , TIDA-00449 , BQ76930 Tool/software: Code Composer Studio I want to communicate with BQSTUDIO with firmware of EV2400 and TIDA-00499
Can you please tell me what to do?
What is…
Part Number: TIDA-00449 Other Parts Discussed in Thread: TIDA-00499 , BQ76920 , BQ76930 , BQ76940 , , BQ76952 , TIDA-010208 , BQ76942 I need to use this BMS system to read battery level and display it on an LCD display.
Is there a circuit board that serves this…
Part Number: THS4521 Other Parts Discussed in Thread: TIDA-00499 , , ADC3441 , TINA-TI , INA149 , TIDA-00049 Hi,
Please help to analysis the attached circuit which is the same with TIDA-00499, but when simulate with TINA, we could find that the output waveform…
Part Number: THS4521 Other Parts Discussed in Thread: TINA-TI , TIDA-00499 Tool/software: TINA-TI or Spice Models hello ,in article “Using fully differential op amps as attenuators, Part 3: Single-ended unipolar input signals” ,there is a ciruit…
Hello
Please see my previous thread where I have recommended TIDA-00499.
TIDA-00499 can be can be interfaced to 25 MHz or 125 MHz pin compatible high speed ADC based on the sampling requirement.
The frontend is customer dependent and you may want to…
Part Number: THS4521 Other Parts Discussed in Thread: TIDA-00499
Now I am troubled by a problem.When my input voltage is particularly large about 3500V,I want to divide the voltage to 0.5V. ths4521-V1P_IN-(-3500V到300V).TSC
but because R2 resistance is…
Part Number: THS4521 Other Parts Discussed in Thread: TINA-TI , , ADC3441 , TIDA-00499 Tool/software: TINA-TI or Spice Models Can anyone tell me what causes the waveform to be so bad, what can be improved to make the waveform normal? ths4521_TIna_NO cap gnd…
Part Number: THS4521 Now I am troubled by a problem.When my input voltage is particularly large about 3500V,I want to divide the voltage to 0.5V. ths4521-V1P_IN-(-3500V到300V).TSC
but because R2 resistance is relatively small, only 52.3 ohms,So the R1…
Hi Yi Xiao,
A good example of LM4140 design is TIDA00499
www.ti.com/.../TIDA-00499
In this TIDA they use a LM4140 in the schematics shown on pg 41 of the user guide.
I would connect the ESR resistor to only one capacitor. I would recommend to have…