Part Number: TIDA-00874 In reference design site ( https://www.ti.com/tool/TIDA-00874#design-products ) the link for the Bill of Material is broken. The reference of the file is below:
Bill of materials (BOM) — TIDA-00874
TIDRJX3.PDF (318 K)
It…
Part Number: TIDA-00874 Other Parts Discussed in Thread: TPA3251
In the schematic file we can see four groups of RC connected between input of TPA3251 and output. What are the purpose of these components? Why are they not placed?
Part Number: TIDA-00874 Other Parts Discussed in Thread: TAS3251EVM , , TAS5805MEVM , MSP430F5529 Hi there,
I was hoping to make up the TIDA-00874 Reference Design as it is exactly what I'm after (The TAS3251EVM is a bit expensive and complicated for…
Part Number: TIDA-00874 Other Parts Discussed in Thread: TAS3251 , TPA3251EVM Is this TIDA-00874 (or similar) fully assembled board developed for testing available? For what price?
Other Parts Discussed in Thread: TIDA-00874 hello,
I would like to use the TIDA-00874 as a base for a own development. Can I get the Schematic files as source files, not only PDF?
I tried to download all related documents, but it ssems tahrt several links…
Hi, For DVDD I would recommend to use a 10uF and 0.1uF, if using the internal LDO a 0.1uF should be enough.
You can also refer to Ref. Design document TIDA-00874 for a sample application.
Regards,
Arash
Other Parts Discussed in Thread: PCM5242 This amplifier reference design measures impressively well. I'm impressed, but have 2 questions. It drives approx. 80 Watts per channel into 4 Ohms at the threshold of clipping. The peak voltage at this threshold…
Hi, thanks for the answers.
Last question, about what you said in the 1st answer. The PCM1690 has a 8V peak-to-peak differential output. The recommended DAC for the TPA3251 (as listed in the datasheet and used in TI made design TIDA-00874) has a 4.2V…