Part Number: TIDA-01401 Other Parts Discussed in Thread: LAUNCHXL-F28379D , , THVD1550 , TMS320F28379D , TIDM-1011 , C2000WARE I am attempting to write code for connecting an Absolute Encoder to LAUNCHXL-F28379D. I am using the TIDA-01401 and LAUNCHXL-F28379D…
Part Number: AM26C32 Other Parts Discussed in Thread: AM26C31 , TIDA-01401 , TIDA-060027 , TIDA-00731 , , THVD1400
Hello Community,
We are designing an end-use case using an AM26C31x pair for our data transmission of upto 4Mhz maximum & 500kHz typical. I…
Part Number: THVD1550 Other Parts Discussed in Thread: TIDA-01401 , Hi team,
My customer has some problems about TIDA-01401 as below.
1.About the description in Page 7.
(1)using R42//R43 with 470pF as a low pass filter to improve the immunity?
(2)using…
Other Parts Discussed in Thread: TIDA-01401 , TIDA-00179 , PGA411-Q1 Tool/software: TI C/C++ Compiler Hello. Can you calculate the crank angle by 1 degree by using TIDA-01401? Also, what should I buy to create TIDA-01401? Thank you for your answer.
Part Number: TIDA-01401 Hello,
Can you suggest a device as functional TIDA-01401 ( RS-485 Interface Reference Design to Absolute Encoders) for test encoders and resolvers. I will use for test and see the position of servo motors. The most I need that Endat…
Part Number: TIDA-01401 Hi TI Engineer:
I have two questions.
1.In many circuit systems, a parallel scheme of resistors and capacitors is used to connect the external earth ground with the internal GND.In this way, the DC is isolated, while the AC…
Hello Wasa-san,
The output power graphs and specifications listed in the datasheet are single ended measurements on the TIDA-01401 board. The TIDA-01401 board, has LMX2594s with optimal, straight and short traces that is good for measuring the power of…
Hello Tachibana-san, all, Schematic and layout reviews are pending. In the meantime I have shared schematic and PCB considerations with Tachibana-san to achieve Class A 4-kV IEC61000-4-4 EFT test pass:
Possible solutions rest on improving the schematic…
Hello Zoe,
This schematic looks good to me. Note that the TPD1E10B06 will break down at 6 V, so you should make sure that normal operating voltages for the RS-485 bus are within this range. (I mention this because it may limit the ground potential…