Part Number: TIDM-1002 Tool/software: Code Composer Studio Hello all,
I'm fairly new with the MSP430 and the Code Composer Studio. Right now I'm following instructions in the TIDM-1002 Reference Design Document. When I try to load the CCS Project from…
Part Number: TIDM-1002 Hello All,
I've a similar issue as the one who started this thread. I would like to make some adjustments in the GUI-software provided with the TIDM-1002.
Are the sources of the PC GUI interface available for download? Can you…
Part Number: TIDM-1002
Tool/software: Code Composer Studio
Hello All,
I'm working with the MSP‑EXP430FR5994 and the Booster board for a few days now but I can't get it working properly. I'm using CCS (Version: 8.1.0.00011) and gas library (Version…
Part Number: TIDM-1002 Dear Champs,
I notice in sec 3.2.2.3 in the doc ( ), it says the minimum flow detection is 7.95 lph, calculated under the maximum flow of 4930lph.
Is "the maximum flow of 4930lph" the limitation of the max flow that can be detected…
I hope I am not doing anything against the forum guidelines if I post another question in this thread since it is connected to the ones by user3983095.
I have noticed that the Absolute TOF provided by the GUI can be smaller than the Gap between pulse…
Part Number: TIDM-1002
I wonder whether the source code for the PC GUI that reads data from the MSP-EXP430FR5994 (and sends the configuration) is open and available somewhere or if it is proprietary. I would like to change how the data is logged and visualized…
Part Number: MSP430FR5994 Other Parts Discussed in Thread: MSP-EXP430FR5994
Tool/software: Code Composer Studio
Hello,
I am Wang Yinsen from Shanghai Zhaofu Electronic Technology Co., Ltd. Recently, my company was researching the ultrasonic gas meter…
Part Number: TIDM-1002 Tool/software: Code Composer Studio Hello TI experts,
I am playing around with the TIDM-1002 Ultrasonic Gas Meter Front-End With MSP430 Reference design. I am trying to build the example project provided with the gasLibrary in Code…
Hello.
In the document "TI Designs: TIDM-1002 Ultrasonic Gas Meter Front End With MSP430™ Reference Design" on page 20 there is "The flowtube design is available as an STL file and may be 3D printed with PLA or ABS." Where i can get STL…