Part Number: DCA1000EVM Although the computer IP address has been configured according to the tutorial, the computer could still not connect to the board via Ethernet. We use Wireshark to record Ethernet packages and found that ARP packages got no response…
Part Number: TMDSCNCD263 Hello Team,
I have an issue with Ethernet transmission, MCAL Eth demo is working.
From my configuration Eth frames are receiving but no transmission.
Q1) Do i need to control MUX via I2C IO Expander?
RGMII_MUX_SEL signal in controlled…
Hi Erik,
Got the confirmation from the team that currently the SD_STORE is not supported.
I thought SD_STORE would be able to help you in this situation, but we're kinda out of luck here.
One last thing I'd suggest you to do is configure the SW2 switch…
Part Number: PROCESSOR-SDK-AM64X Hi,
Customer is evaluating AM64x/AM243x. There is a pinmux conflict using CPSW RGMII/RMII for Gbit Ethernet so they asked if PCIe + Serdes interface can be used instead to communicate with other chips via Gbit ethernet…
Hi,
jin zhu said: I may not have expressed myself clearly, regarding the option to set the voltage, can you tell me in which group it is?
Please refer to Power Domain options form Sysconfig tool.
jin zhu said: I have confirmed that the voltage of the VDDSHV2…
Part Number: PROCESSOR-SDK-AM65X Developed using PROCESSOR-SDK-RTOS-AM65X ver07.03.00.09. NDK is using NDK 3.80.00.19.
I want ethernet ports eth0 and eth2 (ICSSG0 and ICSSG1) to communicate on the same subnet. For example, I want to set eth0 to 192.168…
Hi Tiziana,
Apologies for the delay in my response! I was stuck with other issues as well.
I couldn't find any root cause from above information that you provided. Could you please provide a complete project for debugging at my end, you can send me a…
Part Number: DP83867IR We are using DP83867IR as the ethernet phy in our board with NXP IMX8MP. We have two etherner ports, and the first port works correctly, and the second port does not. So, we tried to debug the issue and took the register dump of the…