Part Number: TLC59116EVM-390 Other Parts Discussed in Thread: TLC59116 Good morning,
I received an eval kit for TLC59116EVM-390 and tried to install the PC software on my Windows 11 machine, but it would not install.
is there a new installer or can I…
Part Number: TLC59116EVM-390 Other Parts Discussed in Thread: USB2ANY , TLC59116 Hello,
We are running into issues with the TLC59116EVM-390. It seems like the web GUI can’t connect to the board. When the board was probed, it seems like voltages across…
Part Number: TLC59116EVM-390 Other Parts Discussed in Thread: TLC59116 , USB2ANY Dear TI expert,
I bought TLC59116EVM-390
And I download the EVM Setup Files for properly install the EVM TLC59116 software
But the device is NOT operational.
I exert 12V for…
Part Number: TLC59116EVM-390 I plan on using your Eval board TLC59116EVM. I am targeting to use Ref Des J6 for the input power to the eval card. However in section 2.1.6 calls out a 3.5-mm diameter connector and section 4.3 calls out a 2.5 mm connector…
Part Number: TLC59116EVM-390 Other Parts Discussed in Thread: TLC59116 To Whom it May Concern,
Why is such a capable voltage regulator, the fast-transient response, 1.5A rated, TPS7A4533KTT used on the eval board? The LEDs are driven by Vin and I do not…
Part Number: TLC59116-Q1 Other Parts Discussed in Thread: TLC59116EVM-390 , Hi TI-team
My customer wants to connect a socket to an TLC59116EVM-390.
(Remove TLC59116PW on TLC59116EVM-390.)
What kind of socket is suitable for TLC59116-Q1 TSSOP (28) ?
Is…