Hi Alfonso,
the schematic is ok as well as the pcb.
It may relate to the device you use.
It is recommended to apply for one of Evaluation board and have a try.
TLV61046AEVM-833 Evaluation board | TI.com
Best Regards
Fergus
Part Number: TLV61046AEVM-833 Other Parts Discussed in Thread: TLV61046A , TPS61093 Hello.
In TLV61046AEVM-833, it is used at Vin = 3V, Vout = 12V, Iload = 80mA.
When Vin = 2.8 V, the output voltage drops.
However, when the input voltage is gradually lowered…
Part Number: TLV61046AEVM-833 Other Parts Discussed in Thread: TLV61046A , TPS61240 Hello! We have TLV61046A EVM. I need help with the following: EVM does not make 5V output with the parameters mentioned in the subject and below. Our circuit goal is the following…