Part Number: TMDSEVM6472
Tool/software: Code Composer Studio
hi
This is my first time usinig CCS..my C code works fine with code blocks however when i try to run it with CCS i got a lot of errors such "
"P_estimate" is not a type name "…
Part Number: TMDSEVM6472 Tool/software: Code Composer Studio Hello,
I am trying to build a DWT ( discrete wavelet transform ) application for TMDSEVM6472 using Code Composer 4
The code is attached below
i get this error "errors encountered during linking…
Part Number: TMDSEVM6472 Hi,
Currently i am using TMDSEVM6472LE and i have selected ADS5474EVM as my ADC evaluation platform. Is there any option (with additional daughter card) i could interface the two platforms?
Regards
San Vs
Hi, Rex
I flashed evmc6472-initramfs-min.el-linux-c6x-2.0.0.63.bin , but it did not help. I n minicom nothing appears. T hough loading Linux from the tftp server is successful. I think the problem is loading procedure the kernel with nand memory. In my i2cConfig…
Hi,
What I've found so far is that the part matches the datasheet recommendations. So it should be possible to be used. However, I'd like to compare it to what's used on the TMDSEVM6472, but I have troubles finding the schematics.
I've asked…
Part Number: TMS320C6457
Hi team, I am posting this on behalf of our customer. They need a development board for TMS320C6457. TMDSEVM6472 EVM that is available in the Design and Development section in its product folder seems not compatible with TMS320C645…
Can you please ensure be the driver support/ configuration support of the ccs 6.x wrt to TMS320TCI6486 EVM and using emulator XDS510 usb emulator.
also does it need .ccxml file or .gel file , how I can get these file for this board.
See http://www.ti…