Part Number: AM3358 Other Parts Discussed in Thread: DA8XX
Tool/software: Linux
Hi,
We interfaced 16bit(565) lcd panel (ET028003DHU having lcd controller HX-8347 I) with our custom board which is based on am335x evm-sk design.
The lcd panel was…
Other Parts Discussed in Thread: AMIC110 , CLOCKTREETOOL , SITARA-DDR-CONFIG-TOOL , AM3352 , AM3351 , AM3357 , AM3356 , AM3354 , AM3359 , AM3358 , AM62L Hi TI Experts,
Can you provide a List of collaterals that can be referred when starting a custom…
Part Number: PROCESSOR-SDK-AM335X Other Parts Discussed in Thread: AM3359
Tool/software: TI C/C++ Compiler
We are working on a custom board based on AM3359 . SDK we are using is ti-processor-sdk-linux-am335x-evm-05.00.00.15 .
This is our
…
Hi Tsvetolin Shulev,
In our Board we are using CS1 for SPI1, But in the above reference the PIN mux given is for CS0 for SPI1
SPI1 - CS0:
(mcasp0_aclkx) - SPI1_SCLK (mcasp0_fsx) - SPI1_D0 (mcasp0_axr0) - SPI1_D1 (mcasp0_ahclkr) - SPI1_CS0
Can…
Hi Pavel Botev,
We are using custom board
Fullscreen
2816.dmesg.txt
Download
root@am335x-evm:/usr/share/qt5/examples/touch/fingerpaint# dmesg
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.19.38-g4dae378bbe…
Other Parts Discussed in Thread: TPS65910 Hi,
I am trying to insert my touchscreen driver module in linux 3.7 kernel for am335x sitara starter kit . In this architecture its look like i have to do modification for board specific changes in dts file…
Part Number: PROCESSOR-SDK-AM335X Other Parts Discussed in Thread: AM3359 , AM3352 , TPS65910
Hi,
We are working on a custom board based on AM3359. Our board is booting successfully and working fine.
But PING is not working and data transfer is…
Hi:
I have a problem about CCSv5.5 in Ubuntu10.04.
I installed the CCSv5.5 successfully.When builting the demo in the AM335x_StarterWare_02_00_00_06,it can create the .out file.But it can not create the .bin and ti.bin files. My configuration is:Property…