Part Number: TMDXICE110 Other Parts Discussed in Thread: SYSBIOS , AM3359 , AMIC110 Previously i asked same question for LED code.
e2e.ti.com/.../tmdxice110-exception-when-loading-code-through-jtag-for-tmdxice110
I have done resolution mention as per link…
Part Number: TMDXICE110 Other Parts Discussed in Thread: AMIC110 Hi,
Is profinet protocol built into this evaluation board? Can customers use it directly? The software directly burns the routine program and then communicates with the board via SPI.
Thanks…
Part Number: TMDXICE110 I'm trying to debug code for TMDXICE110 using XDS110 debugger. following is sequence.
1) Launch iceAMIC110.ccxml configuration.
2) Connect to cortexA8.
3) Do the CPU SW reset.
4) Load out file
Im getting exception : CortxA8…
Part Number: TMDXICE110 Other Parts Discussed in Thread: UNIFLASH , AMIC110
I'm working on TMDXICE110. I'm able to flash & debug code using Jtag. I'm exploring more option to flash code without Jtag So I came across utility uniflash tool. I followed step…
Part Number: TMDXICE110 Other Parts Discussed in Thread: AMIC110 , PROCESSOR-SDK-AMIC110 Hi Team ,
We are in process to buy TMDXICE110 to test industrial protocol like Profinet , Ethernet/IP but most of software link related to development are broken or…
Part Number: TMDXICE110 Im working ICSS_EMAC_Basic Example (ICSS_EMAC_BasicExample_iceAMIC110_wSoCFile_armTestproject) as per description it is EMAC Loopback test at PRU-ICSS EMAC PHY .
software-dl.ti.com/.../index_device_drv.html
I have following queries …
Part Number: TMDXICE110 I followed steps mention in SDK document. following are logs. Highlighted command in bold.
C:\ti\pdk_am335x_1_0_17\packages> pdksetupenv.bat
***************************************************Environment Configuration:******…
Part Number: TMDXICE110 Other Parts Discussed in Thread: AMIC110 Hi
I have some question about TMDXICE110.
https://www.ti.com/tool/TMDXICE110
Q1. I think AMIC110’ s EMAC is pinned out only 1 port.
But the TMDXICE110 seems pinned 2 port.
Is this…
Part Number: TMDXICE110 Hi Team,
Can you help with the inquiry below?
TMDXICE110 is used to run the EtherCAT application demo: ethercat_slave_full_AMIC11x_arm
When the EtherCAT slave is scanned, it can't switch to dc mode.
as the picture shows, there…
Part Number: TMDXICE110 Hi Team,
我用TMDXICE110去跑官方ethercat demo,Twincat连上之后,无法选择是工作在SM模式还是DC模式
这里的模式选择,应该是可以选择为SM模式或者DC模式的
查看COE ONline,发现应该是支持DC模式的:
I used TMDXICE110 to run the official ethercat demo. After Twincat was connected, I cannot choose whether…