Part Number: TMDXLCDK6748 Tool/software: Code Composer Studio Hello my friends. I'm from Russia, looking for some help.
I have a TMDXLCDK6748 development board and try to use mcasp example to check one.
c:\Program Files (x86)\Texas Instruments\pdk_C6748_2_0_0_0…
Part Number: TMDXLCDK6748 Tool/software: Code Composer Studio Dear TI,
I recently started working on tmdxlcdk6748, using ccs.
I want to pass a summed signal of two sine waves and eliminate one of it using fir filter. I produced the sample values of the…
Part Number: TMDXLCDK6748 Tool/software: Code Composer Studio I want to execute a linear convolution program in ccs. There is not error in build. But when I debug, I get the following result.
(I will be putting down the code along with the console too…
Part Number: TMDXLCDK6748 Hi,
How to calculate Power dissipation for processors? Does Power dissipation means the same with Power Consumption for processors?
Part Number: TMDXLCDK6748 Hi
I am using the TMS320C6748 development kit.
Could you tell me which are the differences between CLKMODE = 0 and CLKMODE 1 because looking at the data sheet
Then there are examples of an On-Chip oscillator
And an internal…
Part Number: TMDXLCDK6748 Tool/software: Code Composer Studio Hello,
I am using LCDK6748 evaluation board. And I should make interface to external SPI ADC such as ADS131A04 through expansion connector J15. TMS320C6748 will perform SPI mater role and ADS131A04…
Part Number: TMDXLCDK6748 Tool/software: Code Composer Studio Hi,
How can I write my application to the MMC/SD card in the LCDKC674X development board and run it on the board without connecting to a PC? I wrote an audio DSP code which is working fine…
Part Number: TMDXLCDK6748 Tool/software: Code Composer Studio Hello,
I am running the example program from Donald Reay's book "Digital Signal Processing and Applications with the OMAP-L138 eXperimenter"., specifically the L138_loop_intr.c on…
Part Number: TMDXLCDK6748 Hello,
I want to make my c6748 lcdk output the date and time. Can i do such a thing? Is there and API's that i can find?
Regards
Rabah
Part Number: TMDXLCDK6748 Tool/software: TI C/C++ Compiler I am new to LCDK, I am trying to compile sine wave generation example. Can you guide me as to how to setup the project.
I will appreciate if you can walk me through the procedure to build the…