Part Number: TMDXRM42HDK Tool/software: Code Composer Studio I running a while loop for a clock signal in the main() . But I want get into a interrupt routine with an short serial output when I push S1 (GIOA7) . I don't know how I can realise this when…
Yes, it is not necessary to have the JTAG chips on your board. You can simply have a connector to the JTAG pins and then use a scan controller such as an XDS100V2(14pin), XDS100V2(20pin) or an XDS200 to be the interface between your board and the USB port…
Hello Anthony,
thank you for your answer.
I have this boards:
www.ti.com/.../tmdsrm48hdk
http://www.ti.com/tool/tmdxrm42hdk
I want to flash over the JTAG Header, and communicate over the usbmini connector.
The Problem is when the JTAG Header and the usbmini…
Other Parts Discussed in Thread: RM42L432 , HALCOGEN I'm completely new to both Hercules platform and CCS5.
I'm working on TMDXRM42HDK and I have the following problem.
I've written an as useless as dumb program to start to work with the evaluation…