Part Number: TPS25740B I have a doubt in configuring the TPS25740BEVM-741 . it has two connectors, J7 and J8 for HIPWR and PCTRL configuration. I didn't understand which of those pins to connect to configure it to P1 and H1. Kindly help me config…
Part Number: TPS25740BEVM-741 Hi,
We designing a power bank which supports USB power delivery(Type C and A) ..
Output voltage requirement : 5 to 20 volt….based negoitation..The USB port should support based on the requirement voltage around 5 upto 20…
Part Number: TPS25740BEVM-741 Hi USB Team,
Good afternoon, my customer is interested in the Altium files for the TPS25740B EVM - I noticed these files aren't available in the tool folder, can you provide them over E2E?
Thank you!
Regards,
~John
Other Parts Discussed in Thread: TPS65986EVM Hi,
We are looking for DC power adapters which match's the DC barrel jack for the TI's:1. TPS25740BEVM-741
2.TPS65986EVM.
1…
Hi Naser and Youhao,
We believe the above issues relates to emails we have been sending to TI support, but haven't yet received satisfactory responses.
For the TPS25740BEVM-741 this was originally setup in DCM anyway.
We still find that there is no…
Hi Rahul,
Good morning,
Currently we are designing 2 products.
1) Type-C USB PD supported Power bank.
2) Type-C USB PD supported wall adaptor.
1) Type-C USB PD supported Power bank.
Li-ion battery power range 7.4 to 14.8 V (10A to 20A)
Input charge current…