Part Number: TPS27S100BEVM Hello, I designed the design as shown below using the tps27s100bpwpr IC.
When 28v is applied to vin and the switch is turned on, voltage should appear at vout, but 0.07v is displayed. Is there a problem with the design?
Part Number: TPS27S100BEVM The iMon output for the TPS27S100B PSPICE model does not seem to be working.
Iout is set to 1A.
Imon should output 2V, but it remains 0V.
Part Number: TPS27S100BEVM Other Parts Discussed in Thread: TPS27S100 , TPS1H100-Q1 Hi
Currently we're using TPS1H100BQPW in our design. Could TPS27S100BEVM be used as a direct replacement?
The pinouts looks the same.
Thanks,
Liam
Part Number: TPS27S100BEVM I can't get the TPS27S100B spice model to work with LTspice. Is it encrypted? Is there a unencrypted version, that I can use?
-Henry