Part Number: TPS65983 HI,
I bought a TPS65983EVM from TI store, I have some questions:
I set the board to emulate as a mid power charger adapter(CFG ID#12). I want to change the source PDO from 12V/3A to 12V/2A.
Just only change the maximum current.…
Part Number: TPS65983EVM I’m learn the TPS65983 with the BoosterPack board, but I found it always return “!CMD” to my 4CC command,
I just want to confirm that whether the BoosterPack firmware supports 4CC commands?
If not, could you…
Part Number: TPS65983EVM Hi all,
I bought one TPS65983EVM and one EK-TM4C123GXL but I don't know how to connect them together(pin? to pin?).
Does anyone have documents? Please email to me. Thank you very much.
morris.lin@lyrasemi.com
best regards…
Part Number: TPS65983EVM Does anyone know what TPS65938 chip version is on TPS65983EVM? TPS65983 or TPS65983B?
Thank you very much.
best regards,
Morris
Part Number: TPS65982-EVM Other Parts Discussed in Thread: TPS65986EVM , TPS65981EVM , TPS65981 , TPS65982 I need to make a system for a vehicle, electric skateboard, but those are my first steps with USB Type C
I need charger the battery pack of the skate…
Part Number: TPS65983EVM Hi,
We made our board which has TPS65981 PD controller. After bring-up, I have flashed 5V/2A sink application image into the TPS65981 SPI boot memory. To test its compatibility with PD sourcing device, I have tried working TPS65983…
Part Number: TPS65983 HI Sir
1. Could you help to provide TPS65983EVM;s PJT file ? I would test sink and source mode
2. I saw TPS65983 is NRND ,so this mean we can use TPS65983B instead directly ?
Thanks
But i still can not understand why you said tps65983 can not be used in charger without TBT?
1. My charger works well with the USB-type C PD product. The tablet is USB type-C PD3.0. the PD power negotiation with the tablet is OK.
Battery charging is…
Hello,
You can request more data on the TPS65983-EVM including data sheet, EVM user’s guide and firmware configuration tool from the devices product page on ti.com:
www.ti.com/.../tps65983evm
Thank you,
Eric
Hi Lerry,
You can refer the TPS65983 EVM to get started. It's a great place to start and with minimal changes you can get what the customer is looking for.
Please refer www.ti.com/.../tps65983evm
Thanks,
Rahul