Part Number: TPS7A4701EVM-094 Hey team, I had one of my customers have concerns over a couple EVMs blowing up - see below
"I have purchased two of TPS7A47xxEVM-094 now and both have blown up as soon as 30V was applied. I checked the voltage and it…
Part Number: TPS7A4701EVM-094 Other Parts Discussed in Thread: TPS7A4701-EP , Hi,
Our application is to use this LDO part TPS7A4701-EP in adjustable opration with switching some values on the R2.
Could you help check if R2 Values and Calculated Vout doesn…
Part Number: TPS7A4701EVM-094 Hello,
When using the TPS7A4701EVM at output current of 1A and voltage drop of 4V, is this enough PCB area to dissipate the 4W of heat through the bottom package solder pad and the PCB, or I have to add the heatsink attached…
Part Number: TPS7A4701EVM-094 Hello,
I am using the eval board, with the test setup described in the user guide. However, when the enable jumper is turned to ON it looks like there is a short, the input voltage drops from 12V to 2.5V. Current draw is…
Part Number: TPS7A4701EVM-094 In the user guide for TPS7A4701EVM-094, it mentions "before connecting the input power supplyto the EVM,verify that the output voltage is set to the desired supply voltage(+3 V to +35 V range)and that it is current limited…
Part Number: TPS7A4701EVM-094 Other Parts Discussed in Thread: TPS7A47 , TPS7A4701-EP , 1. What will be the recommended R1, R2 value for a 34v output adjustment?
2. Any recommended type of resistor type/brand?
Regards.
Part Number: TPS61378Q1EVM-060 Other Parts Discussed in Thread: TPS7A4701EVM-094 , Hi team,
Can you provide information on the external dimensions of the TPS61378Q1EVM-060 and TPS7A4701EVM-094
Regards,
Hi Stephen,
Yes you should be able to parallel this device using the NR pin, much like the app note you linked to. The TPS7A47 EVM (part number TPS7A4701EVM-094) is in stock but you are correct that the reference design is not orderable.
Thanks,
- Ste…
Hello,
A good low noise lab supply with multiple outputs should work well. However, you can also use individual LDO's, which is how you would power the device when designing your own board.
TPS7a3001 and TPS7a4901 are good options for the +9V and…